{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the Modicon M241 HSC support periodic meter measurement?
Issue
Does the Modicon M241 HSC support periodic meter measurement?

Product Line
Modicon M241 PLC

Environment
HSC (High Speed Counter) feature in PLC

Resolution
Yes, the Modicon M241 controller supports up to 2 channels using the Fast input that can be setup as period meter.
Periodic measurement calculates the period between two events.

Schneider Electric Nigeria