{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATV630 process drive be programmed for anti jam?
Issue:
ATV630 process drive set up for anti jam.

Product Line:
Altivar ATV630 ATV660 process drives

Environment:
All

Cause:
Anti Jam function Programming

Resolution:
Yes, the ATV630's Anti Jam function allows the pump to execute forward, and then reverse pump rotation cycles. See the attached file for programming assistance.

Schneider Electric Nigeria

Attachment(s)
Anti Jam function on the ATV630 Process drive.pdf [249.54 KB]