{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does the Y mean at the end of the ATS48 part number?
Issue:
N/A

Product Line:
Altistar 48

Environment:
Altistart 48

Cause:
N/A

Resolution:
ATS48 has a control supply and a power supply.

On  the Y range, you have a control supply that is 110-220 and the power supply is 208-690V. Y range is dedicated for the US market, with NEC standard soft starter that must be protected against the current unbalance.  Y range has three current sensors,. There are only 2 on the Q range (one more OLF on the Y range).

On Q range, the control supply is 220-415V and the power supply is 230-415V.

Schneider Electric Nigeria