Search FAQs
What is the maximum number of events for the BMXERT1604 buffer
Issue
The user manual does not state what the maximum nuber of events that the buffer in a BMXERT1604T can hold.
Product Line
BMXERT1604T
Environment
Windows 10
Resolution
The maximum buffer size is (16 events x 255 groups max)= 4080 events.
Each group can have a maximum of 16 events.
Events with the same timestamp will be packed into one (1) group.
If the buffer is filled, it will take 204 CPU scans to clear it.
Note: Because only the events with same time stamps will be packed in one group, the 4080 maximum number of evens in the buffer may never be reached.
The user manual does not state what the maximum nuber of events that the buffer in a BMXERT1604T can hold.
Product Line
BMXERT1604T
Environment
Windows 10
Resolution
The maximum buffer size is (16 events x 255 groups max)= 4080 events.
Each group can have a maximum of 16 events.
Events with the same timestamp will be packed into one (1) group.
If the buffer is filled, it will take 204 CPU scans to clear it.
Note: Because only the events with same time stamps will be packed in one group, the 4080 maximum number of evens in the buffer may never be reached.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: