{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Do our Tesys contactor, overload relay,GV2 breakers comply with NFPA70?
The NFPA means National Fire Protection Association.

The NFPA is not a standard it is mainly best practice to protect against fire.

The NFPA best practice leads to generate

- NEC ( National Electrical Code ) which defines how any electrical product must be installed and what are also the electrical installation rules…

- UL standard as UL508, UL489……

It is normal you do not find for TeSys reference to NFPA as only UL 508 refers to this document.

Our products, which are designed under UL 508, can be used without issue as NFPA and NEC lead to their construction under UL standards.

Unfortunately, we cannot send extract of UL 508 standard ( we cannot copy extract ) but reading the UL 508 you will find in pages 17, 27, 28, and 66 of 372 there is in UL 508 document references to NFPA 70.

There is no product ( in regards to our today knowledge ) which are certified under the NFPA guide, they are only certified under UL 508, UL 489…
 

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.