{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Control Expert (formerly Unity Pro) offer status words that can be used to determine the communication health of an ERIO drop ?
Yes, the following System Words will allow you to see the communication health between the CRP31200 and the CRA31200
%SW172-173   Referred to as ERIO Connection Status
0= Drop is not communicating
1= Drop is communicating


R-71117

Schneider Electric Nigeria