{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are there status words available which will allow me to see module health on the Quantum ERIO network?

Yes, the following System Words will provide the health status of each IO module on the ERIO network.

%SW641-702   Referred to as ERIO Module Health. Refer to Control Expert Help for details which discuss how these words apply.
16 bits of the word represent the 16 potential slots in a Quantum backplane.
0 = unhealthy or not mapped
1 = healthy module.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: