{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the causes and remedy for Err8 fault on the ATV212 or SFD212 drives?
Issue:
ATV212 or SFD212 is showing ERR8 fault code.

Product Line:
Altivar ATV21, ATV212 SFD21 and SFD212 drives

Environment:
All

Cause:
Loss of network or network timeout has occurred.

Resolution:
Err8 means network communication fault error. Try checking the network control devices and cables.
The function can be disabled temporarily for troubleshooting by setting F803 to 0 and F851 to 1. However, please do not leave the network disabled. Once troubleshooting is over, please enable F803 back to 1 and F851 back to 4.

Schneider Electric Nigeria