{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Error importing cert, code: -32" from APC Security Wizard
Issue:
After attempting to import a certificate using the APC Security Wizard, an error is returned stating "Error importing cert, code: -32" 

Product line:
APC Network Management Cards

Environment:
All FW revisions

Cause:
This error is caused by an "unrecognized data format" - an issue with the template used to create the certificate. It has been reported most often when using Microsoft PKI when creating a certificate.

Resolution:
If using Microsoft PKI to generate a certificate, attempt to use the "Web Server" template. It is also possible to create CA root certificates and NMC Certificates using the APC security wizard. Ensure that the information entered on the "Distinguished Name" page matches the certificate. The "common name" should be the IP address or DNS of the Network Management Card.

This issue will be resolved with a future firmware revision, and this article will be updated with the version number when publicly available.. As part of this resolution, a new version of the APC Security Wizard will be launched simultaneously.
 

Schneider Electric Nigeria

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.