{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Machine Expert - Basic and M221 controller : Why the SEND_RECV_ SMS function block returns CommError: 255 with OperError: 16?
Meaning of OperError Codes 16 and 17 when CommError Code is 255 (Message refused):
Value Description
16
The phone number in the received message does not match with the list of approved numbers (whitelist).
17
The received message does not match with any message in the command list. Issued only if the sender phone number matches an entry in the list of approved numbers (whitelist).

Solution:
16 : Write the phone number list with international notation, example: for 0518497647 use 33518497647 where 33 is the international code number of the country.
17 : The received message must be the same as the one configured (Case sensitive).

Schneider Electric Nigeria