{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to configure audible alarms as per different alarm priorities in Vijeo Citect?

Follow below mentioned steps to configure different audible alarms as per alarm priorities.

1. In Citect Project editor open Computer setup editor > under Alarm group add sound<n> parameter.  Browse and select the sound file (in .wav format) as per alarm priority.  Add sound<n>Interval in Ctect.ini. Same way different sound files can be configured as per different alarm priorities.

In Citect Project editor open Computer setup editor

2. Define alarm priority as per different alarm categories.

Define alarm priority as per different alarm categories.

3. Then go to Citect project Editor > Systems > Included Projects and add CSV_Include project.

dd CSV_Include project.

4. Run computer setup wizard and in the Events setup enable CSV_AlarmClient. Then complete the wizard and start runtime.

Run computer setup wizard and in the Events setup enable CSV_AlarmClient.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: