{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can programs created with Modsoft be opened with the ProWORX 32 software?
Issue
Open Modsoft project with ProWORX 32

Product Line
ProWORX 32

Resolution
Yes. Programs created with Modsoft can be imported, then opened, using ProWORX 32 software. With the ProWORX 32 software up and running, go to <FILE> then <IMPORT DATABASE>, select File Type as (*.CFG) for Modsoft, then go into the folder that has the Modsoft *.CFG file and select it, click on the <OPEN> button and the conversion process will begin.

Schneider Electric Nigeria