{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Why are my configuration settings missing after a power cycle on a HMIG5U/HMIG5U2?
Issue:
Configuration settings missing after a power cycle on a HMIG5U/HMIG5U2

Product Line:
HMIG5U, HMIG5U2, Smart iPC, iPC with CFAST or Flash Card as disk drive.

Resolution:
When the EWF (Enhanced Write Filter) is activated for the system drive (C:\ ) on a HMIG5U/HMIG5U2 or any iPC with a Compact Flash card or CFast card as the system drive, any sort of file change or configuration setting made to C:\ will be lost after a power cycle. The only way to retain these changes after a power cycle is to commit them to the disk drive using the EWF configuration tool. Alternatively, you can deactivate the EWF before making any changes.



To deactivate the EWF, please follow this procedure below:

1) In the task tray, look for the icon of a drive and a lock.
2) Click on this icon to open the EWF Configuration Tool.
3) Select the drive letter and press the "Configure" button.
4) Select the drive letter again and notice "Pending command" is activated.
5) Select in the drop down menu "Commit and disable live"
6) Press the "Apply" button and then press the "OK" button.
7) Notice that the EWF is now deactivate.

Once the EWF is deactivated, you can make all your changes to C:\ and they will be retained after a power cycle. Once you are done making changes to the C:\, remember to re-activate the EWF to continue with the system drive protection.

To re-activate the EWF, it is the same process as shown above with the exception that you will now choose to activate the EWF.

 

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.