{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
EGX150 serial communication cable
Issue
User is trying to purchase a cable to wire serial communication to EGX150 (Link150) to downstream devices through its RJ45 serial port

Product Line
EGX150 (Link150)

Environment
Serial communication

Resolution
Part# VW3A8306d30

This cable is for Modbus serial link 1xRJ45, free wires at the other end. 3m length

The correspondence between the wire colors of cable VW3A8306D30 and the pin numbers of the RJ45 socket is as follows:

Wire diagram
Wire Connection Diagram

Schneider Electric Nigeria