{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum motor lead length you can run the ATV320 drive, without a load reactor?
Issue:
What is the max cable length you can run the ATV320 drive?

Product Line:
Altivar 320

Environment:
All

Cause:
Motor cable length distance without a load reactor.

Resolution:
The ATV320 drive can run up to 164 feet without a load reactor.
Cable length can go up to 164 ft without a reactor. If it's shielded cable we can go to 328 ft with a reactor. If it's  unshielded cable we can go up to 656 ft with the reactor.

Cable Characteristics (ATV320 Installation Manual page 75)

If you are using cables longer than 50 m (164 ft) between the drive and the motor, add output filters (for more details refer to the catalog). Use a shielded cable to meet the requirements of Category C2 or C3 according to the standard IEC 61800- 3, except when using a sinus filter. In this case, the use of a non-shielded motor cable is possible.

Schneider Electric Nigeria

Attachment(s)
ATV320_Installation_manual_EN_NVE41289_05-pages-75.pdf [118.58 KB]