{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the cable to use with Bluetooth adapter TCSWAAC13FB to connect to a M221 PLC
The M221 catalog pages advise about M221 compatibility with Bluetooth adapter TCSWAAC13FB
but none of the cables (including the RS485 RJ45 cable) provided within the box of the Bluetooth adapter TCSWAAC13FB is compatible with the RJ45 RS485 serial interface of the M221
It is necessary to have a cable reference XBTZ9980 to connect the TCSWAAC13FB to a M221 PLC


Schneider Electric Nigeria