{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
[Unity Pro V11]How to succeed the application built in case of large size
Question:
Customer came across built error or unity crash after executing “Rebuild all project” for around 2 hours. Application size is huge as 210m.
How to solve it?

Answer:
Once the issue comes from our Database called ObjectStore, the huge application built at Unity Pro has bypassed the limitation of the database which leads to the issue.

Resolution is to increase the amount of memory in registry table allocated to the Database
Attached  is a reg file to change the Database settings
Please double click on it to integrate it into the Windows Registry
Start Unity Pro and perform the test.

Schneider Electric Nigeria

Attachment(s)
Registry_OStore.7z [365 Bytes]