{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Modbus TCP option for an ATV600 series drive?
Issue:
Modbus TCP option for a ATV660

Product Line:
ATV600 series

Environment:
All

Cause:
Product Selection & Services

Resolution:
Modbus TCP is standard in the ATV600 series. There is no separate option card for Modbus TCP in the ATV600 series.

Schneider Electric Nigeria