Search FAQs
PME error "failed to write node info to database because 'The server threw an exception. (Exception from HRESULT - 0x80010105 (RPC_E_SERVERFAULT))'
Issue:
A customer is seeing the following error message within the System Log events.
"failed to write node info to database because 'The server threw an exception. (Exception from HRESULT - 0x80010105 (RPC_E_SERVERFAULT))'. Will retry in 60s.)
Product Line:
SPM 7.0.1 / PME 8.0 / 8.1
Environment:
WIndows server 2008 / 2008 R2 / 2012 / 2012 R2
Cause:
The system has corrupt operating system files.
Resolution:
The system will require either formatting and restoring from back ups or installation on a new machine.
A customer is seeing the following error message within the System Log events.
"failed to write node info to database because 'The server threw an exception. (Exception from HRESULT - 0x80010105 (RPC_E_SERVERFAULT))'. Will retry in 60s.)
Product Line:
SPM 7.0.1 / PME 8.0 / 8.1
Environment:
WIndows server 2008 / 2008 R2 / 2012 / 2012 R2
Cause:
The system has corrupt operating system files.
Resolution:
The system will require either formatting and restoring from back ups or installation on a new machine.
Released for:Schneider Electric Nigeria
Explore more
Product:
Explore more
Product: