Search FAQs
What lengths are available for the control cable and their part numbers for Recloser/LBS?
Issue
Need a longer control cable for my Recloser (N/U/W) or Load Break Switch (RL) then the standard 7 meter control cable.
Product Line
Recloser N/U/W Series
Load Break Switch RL Series
Environment
ordering
Resolution
The control cable length and part numbers are below:
Need a longer control cable for my Recloser (N/U/W) or Load Break Switch (RL) then the standard 7 meter control cable.
Product Line
Recloser N/U/W Series
Load Break Switch RL Series
Environment
ordering
Resolution
The control cable length and part numbers are below:
Length | part number |
11 meters | 992000045 |
12 meters | 992000115 |
15 meters | 992000175 |
20 meters | 992000100 |
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: