{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where is the run command connected on the ATS01...FT?

Article available in these languages: Spanish

Issue:
How is the run command wired to the ATS01...FT Altistart Softstart?

Product Line:
ATS01

Environment:
ATS01...FT

Cause:
Wire diagram not clear

Resolution:
External control voltage must be used.
If 110-240Vac control voltage is used. (can use the line voltage in the line inputs)
CL1/0 (neutral) and CL2 (120Vac) must be applied at the same time as line voltage.
If +24Vdc control voltage is used .
CL1/0 (-) and 24V (+) must be applied at the same time as line voltage.
Refer to manual catalog part number 8637CT0401
NOTE:  A contactor or starter and overload protection are required with these softstarts.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: