{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I run a 460Vac motor on a 575Vac ATV61 or ATV71 drive?
Issue:
Running a 460Vac motor on a 575Vac ATV61/ATV71 drive.

Product Line:
ATV61 ATV71

Environment;
All

Cause:
Test motor 460Vac Line supply 575Vac

Resolution:
No, this is not recommended.
Drives are designed to run motors with the same voltage rating.

Schneider Electric Nigeria