{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can I find the fault history in the ATV32 drive
Issue:
How can I check the fault history in the ATV32 drive?

Product Line:
ATV32, Altivar 32

Environment:
All part numbers, all models

Cause:
Customer wanted to know if drive has a fault.

Resolution:
The fault history is in the Diagnostics menu, and can be accessed using the graphics keypad VW3A1101, or SoMove software.

Schneider Electric Nigeria