{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the hole sizes and dimensions of the AR8395 copper bus bar?
Issue:
A customer wants to use 2-hole lugs on the ground bar

Product Line:
NetShelter Bus Bar

Environment:
AR8395

Cause:
Grounding / bonding is required

Resolution:
The AR8395 has the following holes available:
47 holes threaded #10-32, spaced 18 cm center to center.
25 holes at 5.5 cm and 9 holes at 7.9 cm, spaced at 25 cm center to center.

Schneider Electric Nigeria