{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How can I ensure the class 2 during installation of my Resi9 Electrical Panel ?

If the Electrical Panel is set directly on the wall, there is a need to add an insulated backpart to your base Electrical Panel.
If installed on trunking system or recessed tray there is no need to add additional accessories.

For more details please click : https://www.se.com/ww/fr/fr/download/document/NVE1357501

Schneider Electric Nigeria

How can I ensure the class 2 during installation of my Resi9 Electrical Panel ?

If the Electrical Panel is set directly on the wall, there is a need to add an insulated backpart to your base Electrical Panel.
If installed on trunking system or recessed tray there is no need to add additional accessories.

For more details please click : http://www.schneider-electric.com/fr/FR/download/document/NVE1357501

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
move-arrow-top