{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert (PME) 8.1 Vista Hotfix 16147.3

Issue

The following issues relating to Vista are addressed in this Hotfix:

  1. When an event was acknowledged in the Vista Global Event Viewer, the cursor would change to an hourglass and stay like that until Vista is restarted.
  2. The Vista scrolling graph display object would leak memory, so if a Vista diagram that includes this type of object was left open for an extended period of time, Vista would eventually crash.
  3. The number of data log viewers in a single Vista diagram was limited to the hard-coded value of 60. This has been increased to 100.
  4. The Vista menu item 'Alert on Comm Errors for Disabled Devices' did not work as expected. Even if this option was unchecked, you would still see a popup warning dialog if a diagram with objects linked to a disabled device is opened.


Product Line
PME 8.1

Cause
The Vista application will need to be updated.

Environment
Vista Application

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location
that will not be overwritten (i.e. the Desktop).

The attached hotfix can only be applied on a PME 8.1 system.
If the software installation is PME 8.0, it will need to be upgraded to PME 8.1 before proceeding. Installation files for PME 8.1 can be found in FA328586.

Once the system is at version 8.1, replace the vista.exe file in the  "...\system\bin" directory with the one supplied in the attached hotfix file.

NOTE: The hot fix should be applied on the primary/application server and all engineering clients.

Schneider Electric Nigeria

Attachment(s)
[PME81][Hotfix][Vista]_8.1.16147.3.zip [1.38 MB]