{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to resolve an ILF condition on an ATV71 Ethernet IP option card (VW3A3320) while running Angry IP Scanner tool?
Issue:
How to resolve an ILF condition on an ATV71 Ethernet IP option card (VW3A3320) while running Angry IP Scanner tool?

Product Line:
ATV61 and ATV71 drives with Ethernet IP option card

Environment:
Issue occurs when running a network scanning tool, in this case Angry IP Scanner.

Cause:
A setting in the Scanner generated the fault

Resolution:
Edit the functions running in the scanner and disable or turn off one labeled Web detect.
In Angry IP this can be found under the Select Fetchers set up screen as shown below.
Removing this function from the list prevented the drives from tripping on ILF.

Schneider Electric Nigeria

Attachment(s)
Fetchers_AngryIPScanner.png [29.16 KB]
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.