{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can a 63.75" tall PDU be installed into a 38U NetShelter CX cabinet?

Issue:
The 63.75" tall PDU does not fit onto the accessory rail. Will it fit anywhere else inside the cabinet?

Product Line:
NetShelter CX

Environment:
AR4038A, AR4038IA

Cause:
One of the 63.75" tall PDUs has been specc'd into a 38U NetShelter CX cabinet.

Resolution:
Yes, the 63.75" tall PDUs can attach to the rear mounting rail. Please see the attached file for mounting instructions.

Schneider Electric Nigeria

Attachment(s)

20160729 Tall PDU Mounting Into 38U NetShelter CX.docx20160729 Tall PDU Mounting Into 38U NetShelter CX.docx [5.95 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: