Search FAQs
What is the difference between the Altivar 630 drive and the Altivar 930 drive?
Issue:
Difference between the Altivar 630 and the Altivar 930 drives?
Product Line:
Altivar 630 and Altivar 930 Series
Environment:
All serial numbers for Altivar 630 and Altivar 930 Series
Cause:
N/A
Resolution:
-The Altivar 630 is designed for Variable torque application similar to the Altivar 61 drives and includes a lot of additional pump control and monitoring functions.
-The Altivar 930 is designed for the Constant torque applications and built for the heavy machinery applications similar to the Altivar 71 drives.
-Click on each link above to access the installation manual for the ATV630 Drive and the ATV930 Drive to see more detailed features between the two drives. Also note that the ATV630 has built in Ethernet TCP-IP and the ATV930 Drive has built in Ethernet TCP-IP and Ethernet IP.
Difference between the Altivar 630 and the Altivar 930 drives?
Product Line:
Altivar 630 and Altivar 930 Series
Environment:
All serial numbers for Altivar 630 and Altivar 930 Series
Cause:
N/A
Resolution:
-The Altivar 630 is designed for Variable torque application similar to the Altivar 61 drives and includes a lot of additional pump control and monitoring functions.
-The Altivar 930 is designed for the Constant torque applications and built for the heavy machinery applications similar to the Altivar 71 drives.
-Click on each link above to access the installation manual for the ATV630 Drive and the ATV930 Drive to see more detailed features between the two drives. Also note that the ATV630 has built in Ethernet TCP-IP and the ATV930 Drive has built in Ethernet TCP-IP and Ethernet IP.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: