{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is there an intermediate switch mechanism for the Zen series?

Yes, there is an intermediate switch mechanism for Saturn Zen. The part number is 60PBI.

Some of the key features are:
  • No LED Indication
  • Intermediate Push-button
  • 10AX load
For further information please visit http://www.clipsal.com/Trade/Products/ProductDetail?catno=60PBI
60PBI device image

Schneider Electric Nigeria