Issue:
ATV61 can I set the up / down arrow buttons for + /- speed?
Product Line:
Altivar Machines, Altivar 61, Altivar 71
Environment:
All models and serial numbers
Cause:
Installation / Setup
Resolution:
No, however, in the ATV61 or ATV71 Command Menu / F1 - F4 Key Assignments can be configured for (+) / (-) speeds on the removable HMI.
ATV61 can I set the up / down arrow buttons for + /- speed?
Product Line:
Altivar Machines, Altivar 61, Altivar 71
Environment:
All models and serial numbers
Cause:
Installation / Setup
Resolution:
No, however, in the ATV61 or ATV71 Command Menu / F1 - F4 Key Assignments can be configured for (+) / (-) speeds on the removable HMI.
Released for:Schneider Electric Nigeria