{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to setup an ATV630 Process drive to follow AI2 instead of AI1 as reference?
Issue:
Wants to setup an ATV630 Process drive to follow AI2 (Analog Input 2), instead of AI1 as reference.

Product Line:
ATV630, Altivar Process

Resolution:



From the Main Menu:
  1. Scroll down and select menu 5 Complete Settings
  2. Scroll down and select menu 5.5 Command and Reference
  3. Select Ref Freq 1 Config and assign it to AI2
  4. Unless an HOA (Hand Off Auto) function is used, set Ref 1B switching to [Ref Freq channel 1]
  5. Also set Freq Switch Assign to [Ref Freq Channel 1].

Schneider Electric Nigeria