undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Unity Pro: Can connection modes be selected?
Issue
There is a need for logging in without the ability to make online edits, but the software defaults to programming mode.

Product line
Unity Pro, Control Expert

Resolution
Unity can be configured to prompt for connection mode so that the programmer can select what he desires. Below are definitions of the choices.

"Use Programming Mode" is the default.  It connects the terminal to the PLC
in programming mode.  If another user is logged into the PLC as the programmer,
the user is offered the option to connect in monitor mode.

"Mandatory Programming Mode".  The terminal connects to the PLC. If another user
is logged into the PLC, the connection is refused, no monitor mode offer is made.

"Use Monitoring Mode". The terminal connect to the PLC in Monitoring only mode.

Schneider Electric Nigeria

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.