{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is it possible to increase the lifespan of the Magelis / Harmony HMI screen by turning down the brightness?

Issue:
Is it possible to increase the lifespan of the Magelis / Harmony HMI screen by turning down the brightness?

Product Line:
XBTGC/GK/GT, HMIGTO/GTU/STO/STU, Box PC, Panel PC, Magelis, HMI, life cycle

Resolution:
When current applied the backlight is decreased, lifetime will be extended.  However, power is always provided to the LCD panel, even if LCD entering Standby and Sleep mode.  Therefore, there is no way to extend the lifetime of the screen.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: