{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does 410 at the end of the ATV312 part number mean? Example: ATV312HD11N4410.
Issue:
"410" Suffix on the ATV312HD11N4410.

Product Line:
ATV312

Environment:
Part numbers ending in 410

Cause:
N/A

Resolution:
This is a custom modified version of the ATV312 that is only sold to the customer who had it customized.
A standard ATV312 will not work in it's place.  It has to be ordered through the OEM.

Schneider Electric Nigeria