{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ENM Monitoring and Diagnostics pages display "[Invalid Date]" for timestamps
Issue

The Event Notification Module Monitoring and Diagnostics pages display "[Invalid Date]" for timestamp columns instead of the timestamp.

Environment

PowerSCADA Expert 8.1, Power Monitoring Expert 8.1

Product Line


ENM 8.3, ENM 8.3.1, ENM 8.3.2

Cause

Some local settings use special characters for "AM" and "PM" time notation.  This has been observed with Italian (Switzerland) and Chinese (Singapore).  When Windows is configured to use one of those locales, the code that renders the timestamps in the Monitoring and Diasgostics pages will not be able to properly format the timestamp and will, instead, show "[Invalid Date]".

Resolution

Changing the Windows locale can correct this behavior. For example, Italian (Italy) or Chinese (China) would be sutible replacements for the indicated locales.  These settings can be found under 'Region and Language' in the Windows Control Panel.

Schneider Electric Nigeria