{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the RFI filter grounding jumper for the ATV61HC11N4 Drives?
Issue:
Part number for the RFI filter grounding jumper for the ATV61HC11N4 Drives?

Product Line:
Altivar ATV61

Environment:
Only Frame size 9 ATV61 or ATV71 drives

Cause:
Customer removed and lost the RFI filter ground jumper and need to get a replacement.

Resolution:

The RFI jumper is included as part  of a Field Services only order kit part VY1A1303.

This part only can be ordered thru field services only.

I have attached a sheet of all of the parts that are included in the VY1A1303 kit.    The jumper part is not sold by its self.

This kit applies to Size 9 ATV61 and ATV71 drives only which are the  ATV61HC11N4, ATV61HD90N4 and ATV71HD90N4

Schneider Electric Nigeria