Search FAQs
How do I remove the Front Cover on Altivar Process Drive?
Issue:
Removing the Front Cover on the smaller size Altivar Process Drive.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
Need to access control terminals for wiring
Resolution:
Procedure to Remove the Front Cover of the Drive
Removing the Front Cover on the smaller size Altivar Process Drive.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
Need to access control terminals for wiring
Resolution:
Procedure to Remove the Front Cover of the Drive
- Unscrew the four screws attaching the front cover
- Slide down the front cover
- Remove the front cover
- You can now access control terminals, Modbus and Ethernet ports
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Product:
Range:
Explore more
Product:
Range: