{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How for MBP_MSTR modbus plus function block to read from modbus plus network devices ?
Here is example shown to read device addresses from MB+ devices over network using MBP_MSTR function through MB+ protoocol.
It can be implemented with two steps process by defining all control word and using mbp_mstr function block.
An application is attached for reference.


Schneider Electric Nigeria

Attachment(s)
mobusplus sample mbp_mstr.zef [43.46 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: