{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Magelis HMI connect to a wireless network to use Vijeo Design'Air?
Issue:
Can the Magelis HMI connect to a wireless network to use Vijeo Design'Air?

Product Line:
XBTGC/GK/GT, HMIGTO/GTU/STO/STU, HMISCU, iPC, Box/Panel PC

Environment:
Human Machine Interfaces (HMI)

Resolution:
Yes, the Harmony / Magelis HMI families can connect onto a wireless network.  The Harmony / Magelis HMI needs to be connected to a wireless router or access point and not a USB wireless adapter.
The ports required forwarded by the router are by default:
Data Sharing Port: 6000
Vijeo Design'Air Port: 6002

These can be set differently from the application under the Target > Remote Access settings page:
Remote Access settings page

Schneider Electric Nigeria