{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the remote mount keypad for the ATV12 drives?

Article available in these languages: Spanish, Japanese

Issue:
Part number for remote mount keypad for the ATV12.

Product line:
ATV12, Altivar 12

Environment:
All serial numbers

Cause:
N/A

Resolution:
There are two keypad options: VW3A1006 (IP54) or the VW3A1007 (IP65).
The kit comes with the screws to mount the keypad to an enclosure or door.  A cable to connect the keypad to the drive is not included.  Customer needs to order cable VW3A1104R10 (1 meter) or VW3A1104R30 (3 meter) separately.



Schneider Electric Nigeria