{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does Obr mean on Drive Status display when ramping down on ATV61 and ATV71?
Issue:
Why does my drive show Obr on display when ramping down on ATV61 or ATV71?

Product Line:
ATV61, ATV71, Altivar 61, Altivar 71

Environment:
All

Cause:
N/A

Resolution:
Obr [Overbreaking]  is a drive state and not a fault. It is displayed in the top left corner of the graphic keypad if the drive is decelerating and using the Auto-Adapted Deceleration Ramp to avoid a possible overbreaking fault (ObF). This status may show up when Decel Ramp Adapt parameter is enabled.

Schneider Electric Nigeria