Uninstalling Unity Pro
The following table shows how to uninstall Unity Pro manually:
The following table shows how to uninstall Unity Pro manually:
Step | Action |
1 | Click Start - Program - Schneider Electric - SoCollaborative -, Unity Pro - Remove Unity Pro xx (xx refers to Unity Pro package). |
2 | The installation wizard is launched, Unity Pro starts being removed. |
3 | When the uninstallation of Unity Pro is completed, select the installed drivers and click Remove. When the uninstallation of Unity Pro is completed select, in the same manner, the installed drivers, and DTMs and click Remove. |
Replacing Unity Pro with a Former Version
To install a previous version of Unity Pro, the current version must be uninstalled using the Windows control panel as previously described.
In addition, the following directories must be manually removed:
- Windows 7 (32 bits):
- C:\Program Files\Common Files\Schneider Electric Shared\Tlb
- C:\Program Files\Common Files\Schneider Electric Shared\Common
- C:\Program Files\Common Files\Schneider Electric Shared\SRCSDK
- C:\Program Files\Common Files\Schneider Electric Shared\SSTA
- Windows 7 (64 bits):
- C:\Program Files (x86)\Common Files\Schneider Electric Shared\Tlb
- C:\Program Files (x86)\Common Files\Schneider Electric Shared\Common
- C:\Program Files (x86)\Common Files\Schneider Electric Shared\SRCSDK
- C:\Program Files (x86)\Common Files\Schneider Electric Shared\SSTA
Released for:Schneider Electric Nigeria