Search FAQs
Does Vijeo Designer Support the Allen Bradley Micro800 series PLCs?
Issue:
Unable to find documentation regarding support for the Allen Bradley Micro800 series in Vijeo Designer.
Product Line:
Vijeo Designer (all versions)
Resolution:
Vijeo Designer currently does not support the Allen Bradley Micro800 series of PLCs natively. In order to program a Magelis HMI to talk to the Allen Bradley Micro800 series of PLC, we must use the Modbus TCP/IP protocol. In other words, the Modbus Communication module must be installed on the Allen Bradley Micro800 PLC and the Vijeo Designer application must use the Modbus TCP/IP driver.
Unable to find documentation regarding support for the Allen Bradley Micro800 series in Vijeo Designer.
Product Line:
Vijeo Designer (all versions)
Resolution:
Vijeo Designer currently does not support the Allen Bradley Micro800 series of PLCs natively. In order to program a Magelis HMI to talk to the Allen Bradley Micro800 series of PLC, we must use the Modbus TCP/IP protocol. In other words, the Modbus Communication module must be installed on the Allen Bradley Micro800 PLC and the Vijeo Designer application must use the Modbus TCP/IP driver.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: