{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
M221 Replacement Connectors
Issue:
What are the part numbers for the M221 connectors.

Product line:
TM221

Cause:
Either missing connectors or need connectors to be wired up before the system arrives for install.

Resolution:
TMAT2CSET - connector set for M221C - IO
TMAT2MSET - connector set for M221M and TM3 - IO
TMAT2MSETG - connector set for M221M and TM3 - IO Spring
TMAT2PSET - connector set for M2X1 - power supply

Schneider Electric Nigeria