{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you update the OPC tag list for a meter which has been replaced with a difference device type?
Issue
A customer has replaced a meter in the system with a different meter type and now the OPC tag list is incorrect.

Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
ION OPC service

Cause
The file 'DefaultMeasurements.xml' contains the complete list of OPC tags from all available device types.  This file is located in the directory below, by default.

C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\IONServices

When the 'Update OPC server' command is run from the Management Console this reviews all current system devices and creates the file 'IONServicesConfiguration.xml' within the config\IONServices directory.  The file and IONServices folder do not exist until the 'Update OPC Server' command is run for the first time.  This file will contain the initial device type and must be updated to reflect the new device type.

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

1) Rename the original 'IONServicesConfiguration.xml' file by adding -old to the end of the file name.
2) Ensure the meter is set to the new device type within the Devices section of the Management Console.
3) Run the 'Update OPC Server' command from the Management Console to designate the new correct device type template for the meter.
4) Confirm the tags have been updated correctly by viewing the device through the ION OPC Test client within the system/bin directory.

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: