{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How is the OPR parameter scaled on the ATV71 series drive?

Article available in these languages: Spanish

Issue:
Scaling the Analog Output when using Output Power on an ATV61/71.

Product Line:
ATV61/ATV71

Environment:
All models, All serial numbers

Cause:
N/A

Resolution:
The output power (OPR) function is scaled between 0 and 2.5X the NPR (Rated motor power) setting under menu 1.1 (Simply Start).   This parameter should be set to match the horsepower or KW rating of your motor in order for the output scaling to be accurate.

Schneider Electric Nigeria