{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the tolerance of the voltage range for signaling products?
According to our voltage tolerance design rule,  the allow tolerance of DC products is around 85% to 120%. the allow voltage range of AC products is around 90Vac ~ 264V ac, if the supportable AC voltage is 110Vac and 240Vac in our catalog.

Schneider Electric Nigeria