{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a Marine certification available for the ATV630 or ATV650 Series Drives?
Issue:
Could not fine Marine certification for Altivar 630 or Altivar 650 process drives.

Product Line:
Altivar Machines, Altivar 630, Altivar 650

Environment:
All

Cause:
N/A

Resolution:
Yes, please see attached DNV Certificate.

Schneider Electric Nigeria

Attachment(s)
ATV630 Marine Cert TAE0000175.pdf [233.56 KB]