{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the sheet metal thickness for Prisma iPM System L?
For Prisma iPM system L, the sheet metal thicknesses are as follows:
PaK Back plate1.2 mm
PaK pillars1.5 mm
PaK Side panels1.2 mm
PaK Top / bottom panels 1.2 mm
PaK Front frame1 mm
PaK Front plates --> 1 mm
PaK Door --> 1.2 mm

Full Kit Back plate --> 1.2 mm
Full Kit pillars --> 1.5 mm
Full Kit Side panels --> 1.2 mm
Full Kit Top / bottom panels --> 1.2 mm
Full Kit Front frame --> 1 mm
Full Kit Front plates --> 1 mm
Full Kit Door --> 1.2 mm

Schneider Electric Nigeria